CW 10.3 with P1010 QorIQ - Unknown Error(Empty Text)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW 10.3 with P1010 QorIQ - Unknown Error(Empty Text)

跳至解决方案
1,577 次查看
franka
Contributor III

I'm using CW 10.3 with P1010 QorIQ.  When I try to debug my project today, I get this error - Failed to launch application Unknown Error(Empty Text).  Everything worked fine yesterday but today I can't get past this error.  I've restarted CW and tried a simple hello world application but I always get the same Unknown Error(Empty Text).  What does "Empty Text" mean and where should I look to try to fix this error?

标签 (1)
0 项奖励
回复
1 解答
1,424 次查看
franka
Contributor III

Hi lunminliang,

There were some messages with the logging enabled but they gave me no indication of what was wrong.

Anyway, I figured it out.  I had an evaluation copy of CodeWarrior I was using and I bought the full version but I never obtained the license file because the eval version was working okay.  The eval version must have expired over the weekend.  I went to the "Secure Applications", "Software Licensing" and obtained the license.dat file and put that in Freescale/CodeWarrior/../PA.  Apparently, when the evaluation license expires this Empty Text error must occur when trying to debug.  I can now use Run->Debug Configurations.

Frank

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,424 次查看
lunminliang
NXP Employee
NXP Employee

Is there any log information if you enable CCS log from

"Run->Debug Configurations-><project>-core0_RAM_<processor>-Connect(Download)->Edit...

->Advanced->Advanced CCS setting->Enable logging" ?

0 项奖励
回复
1,425 次查看
franka
Contributor III

Hi lunminliang,

There were some messages with the logging enabled but they gave me no indication of what was wrong.

Anyway, I figured it out.  I had an evaluation copy of CodeWarrior I was using and I bought the full version but I never obtained the license file because the eval version was working okay.  The eval version must have expired over the weekend.  I went to the "Secure Applications", "Software Licensing" and obtained the license.dat file and put that in Freescale/CodeWarrior/../PA.  Apparently, when the evaluation license expires this Empty Text error must occur when trying to debug.  I can now use Run->Debug Configurations.

Frank

0 项奖励
回复