Hi, If you would like to use processor expert for S12XHY family, you should install Codewarrior v5.1 and the patch of CW12_V5_1_PE_V3_05_SP.exe, NOT use Codewarrior v5.2 which does not support it. CW12_V5_1_PE_V3_05_SP.exe could be gotten through the link. S12GA48 Device Initialization Codewarrior 5.1 could be gotten through the link. http://www.nxp.com/lgfiles/devsuites/HC12/CW_HC12_v5.1_SPECIAL.exe
Classic - How to use HCS12 on Eclipse? -build and debug a CodeWarrior project- Valid for some Classic versions - CW for MCU V6.x, CW for HC12 V5.1, etc ... Configuration used: Software Native installation Win 7 Enterprise 64 bit CodeWarrior HC12 v5.1 CodeWarrior for MCU V10.6.4 (Updates 5&6) Hardware S12XDT512 Multilink Universal rev B Introduction Since 2010 we started to move our development tool chains from Classic IDE to Eclipse. However we continue to use classic tools for some products as CW for HC12 V5.x for HCs12 devices. The advantage of HC12 is that all features are used in command line in the IDE. So we can use another IDE than CodeWarrior IDE as Eclipse for instance. This doc will show you how to: - Create a new project using CW HC12 build tools chain, - Define the external debugger to debug the HC12 application. Attached you will find: - a zip file including the projects. Recommend to unzip it to c:\temp, - 2 videos explaining Build and Debug processes. More references/information can be found at: https://community.freescale.com/message/364157#364157 http://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/ NOTE: For Classic versions using integrated debugger, only the build operation can be done under Eclipse. When the debugger is not available as standalone version there is no way to define an External Tools in Eclipse. Phase 1: Create a Project under Eclipse based on a HC12 project 1- Create a project for the device you need under HC12 v5.1. 2- Launch Eclipse and create a new empty project File ¦ New ¦ Other … Enable Show All Wizards and select the C Project (which is otherwise hidden), pressing Next. Click OK Specify the project name, select an Empty Project under Makefile project with — Other Toolchain — and press Finish: Now I have an empty project Using Project ¦ Properties specify my Build Command: ${system:ECLIPSE_HOME}/../gnu/bin/mingw32-make -j6 3- Copy all HC12 V5.1 Sources and config files to Eclipse project 4- Create a makefile with the menu File ¦ New ¦ Other... ¦ General ¦ File Phase 2: Build the project using HC12 build tools chain with makefile 1- Generate the Commandlines used by HC12 v5.1 to build the project. By this way you will have the options and other paths used for compiler and linker to build the project. We can use these information to create the makefile. 2- Create the makefile with the menu menu File ¦ New ¦ Other... ¦ General ¦ File An empty makefile is created. You need to create your makefile according to your project. For more details we recommend to refer to the link: http://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/ This is the makefile created for this example. The makefile created contains 2 operations: all -> build the project and generate Srecord files clean -> remove all generated files 3- Create 2 make targets for all and clean operations with the "Make Target" under Window ¦ show View Now I can build the project using HC12 v5.1 tools (compiler/Linker) under Eclipse project Phase 3: Add External debugger to debug hc12 application HC12 V5.1 is using an external debugger named Hiwave. This tool is using a config file named .ini. To use HiWave under Eclipse project, we need to define it as external Debugger. By the Run menu click on External Tools ¦ External Tools Configuration… Run will launch the Debugger and the project.ini file will be generated in the \Bin folder You can edit the ini file and use the info provided in the .ini file of HC12 V5.1 project To use these settings, add the Arguments: project.abs -w -Target=icd12 -Prod=project.ini Now the debugger is launched and application loaded on board with Multilink Interface.
Classic - How to use dashboard (Jenkins) to build a CodeWarrior project? Valid for all Classic IDE versions - CW for MCU V6.x, CW for PA V8.8, etc ... Configuration used: Native installation Win 7 Enterprise 64 bit Jenkins ver 1.624. https://wiki.jenkins-ci.org/display/JENKINS/Meet+Jenkins http://jenkins-ci.org/content/windows-installers-are-now-available Multiple CodeWarrior installations including CW for MGT V9.2 Example based on CW for MGT V9.2 You should have installed Jenkins (V1.624 for this note) and CW for MGT V9.2 or any other classic versions. When the Jenkins installation is finished, the IE is automatically launched with http://localhost:8080/ To start Jenkins under IE I should plug it under http://localhost:8080/ Note: If you can not access to the web page, you must check than Jenkins service is running. Open a Command Prompt and go to C:\Program Files (x86)\Jenkins Here you can type: Net stop Jenkins Net start Jenkins To avoid problem I've manually removed the project under C:\Program Files (x86)\Jenkins folder and performed from menu: Jenkins + Manage Jenkins + Reload configuration from disk By this way I've a clean installation. Now I've created a new item where I defined the project and added the dir command to be sure Jenkins is using the right path. I copied and extracted the zip file (Jenkins_command_line.zip) in the workspace created. Check the .bat file is correctly configured for your PC installation (CodeWarrior Folder). If you execute the bat file, it should work fine outside Jenkins too. If it's not the case you must review the .bat file. After that I added a new build step for my_test.bat. Now when I clicked on Build Now, the my_test.bat is executed. Attached a video showing the process, this doc in word doc, and the example I'm using
Get “IDE failed to start …” message A- Description In some case after to have installed Classic version, you could meet an error when you launch the IDE. Most of the time the error is introduced because the IDE is not correctly registered. As suggested by the message we need to execute the \bin\regservers.bat file. This will initialize correctly the dlls used by the IDE. In some case, most of the time under 64 bit OS (Win 7 and Win 8), the \bin\regservers.bat generates some errors: B- Solution To solve the problem we need to execute the \bin\regservers.bat file via a Command Prompt running as Administrator mode. Now we can launch the IDE Attached a video showing the process. Hope this will help.
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel)
----
FTL stack trace ("~" means nesting-related):
- Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1]
- Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1]
----
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel)
----
FTL stack trace ("~" means nesting-related):
- Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1]
- Reached through: #include "language_macro_header.ftl" [in template "Language_CP_BulkTranslation_Angular" at line 33, column 5]
----
The following has evaluated to null or missing:
==> translatorRole [in template "Language_CP_BulkTranslation_Angular" at line 36, column 14]
----
Tip: If the failing expression is known to be legally refer to something that's sometimes null or missing, either specify a default value like myOptionalVar!myDefault, or use <#if myOptionalVar??>when-present<#else>when-missing#if>. (These only cover the last step of the expression; to cover the whole expression, use parenthesis: (myOptionalVar.foo)!myDefault, (myOptionalVar.foo)??
----
----
FTL stack trace ("~" means nesting-related):
- Failed at: #if translatorRole == "" || roleStatu... [in template "Language_CP_BulkTranslation_Angular" at line 36, column 9]
----