new to dsp and code warrior, possible memory issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

new to dsp and code warrior, possible memory issues

1,829 次查看
jhall
Contributor II
in the project i'm working on (given to me in a heated rush as the original engineer dashed) i have ~ 89K bytes that is being downloaded when i program my dsp 56858 through J-TAG. the code downloads fine, but when the code is accessed, it crashes.  i then take out unneeded peices of my code for certain debugging to drop the download to ~86Kbytes and once again run the code. this time the code runs fine. i am certain that the functions i commented out to reduce the code size are correct. what i think is happening is that the code is stomping on it's self because i'm over the limit. but i was under the impression that i had 128Kbytes...any help on this? i have attached my map file. thanks for any help!!!
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

628 次查看
trytohelp
NXP Employee
NXP Employee
Hi,
 
This question seems be to be to complex.
Can I suggest you to report it to the support team ?
please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - If you are already registered with Freescale (using the Forum, subscribed to newsletter, ...)  use your Freescale login and password.
    Otherwise, Click on "Register Now" to get registered.
  - You can submit your request through the web from there.
Regards
Pascal
0 项奖励
回复