How do you feel with Code Warrior 8.1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do you feel with Code Warrior 8.1?

2,151件の閲覧回数
rbonacina
Contributor I
Hello, I am currently using Code Warrior 6.1.2 for 56800/E, and I would like to upgrade to the latest version (8.1) in order to have the possibility to develop for DSC's not supported by 6.1.2 (for example: 56F8367). Before doing so, I would like to hear opinions about Code Warrior 8.1 for 56800/E: how do you feel with it? Regards, Roberto
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,181件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
CodeWarrior for DSC 8.0 can be downloaded on our web site.
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600612247

The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.

A patch Version 8.1 is available too.This is a patch for the DSC8.0 (must be installed in first)
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882140B

 
Regards
Pascal
0 件の賞賛
返信