Where are the Processor Expert Examples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where are the Processor Expert Examples

2,411 Views
Geoff_L
Contributor I

I'm just getting started with Codewarrior, and trying to use Processor Expert.    The manul says that PE has built-in examples, but I just can't find them with all of my trying.  Can someone point me in the right direction?

 

I'm using the following CodeWarrior version, targeting MC9S08AC60

 

CodeWarrior Development Studio for Microcontrollers

 

Version: 10.0

Build: 100621

Labels (1)
0 Kudos
Reply
2 Replies

1,730 Views
ProcessorExpert
Senior Contributor III
Hello,
  
we are sorry for the inconvenience, missing Processor Expert example projects will be added into CW V10.1. For now you as workaround please use enclosed projects.
best regards
Vojtech Filip
Processor Expert Support Team
0 Kudos
Reply

1,730 Views
AndyMoran
NXP Employee
NXP Employee

I can open and build these example projects, but I can't figure out how to get the QE to show up in the Components Library or the Target CPU library.  Is there a setting somewhere that I need to set?

0 Kudos
Reply