USBDM-SWD on Windows 10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM-SWD on Windows 10

ソリューションへジャンプ
3,524件の閲覧回数
giallino
Contributor I

Hi all,

is it possible to use the USBDM (I have a Wytec unit based on PGO's JS16 USBDM-SWD design

with 4.12 Firmware) under Window 10 home editions OS and Codewarrior 5.1 for HCS12?

Any help will be very appreciated.

Thank you all.

 

USBDM-SWD

ラベル(1)
0 件の賞賛
返信
1 解決策
2,347件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Coti,

From the the CW 5.1 Release , we can see that the CW 5.1 not support the Win 10.

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,347件の閲覧回数
ryanleis
Contributor I

is there anyway we can use USBDM on windows10? I know Microsoft sucks bigtime but we're needing help bad for our projects...!

0 件の賞賛
返信
2,347件の閲覧回数
RodneyMcGee
Contributor IV

Also use CW5.2 and add your missing devices using this

Add missing derivatives to CodeWarrior 5.2 (Unofficial Method)

CodeWarrior HCS12(X) 5.1 Windows 10 x64 Install and Update USBDM - YouTube

Check out this video, the steps are pretty much the same for 5.2.

0 件の賞賛
返信
2,348件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Coti,

From the the CW 5.1 Release , we can see that the CW 5.1 not support the Win 10.

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信