USBDM-SWD on Windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM-SWD on Windows 10

Jump to solution
3,523 Views
giallino
Contributor I

Hi all,

is it possible to use the USBDM (I have a Wytec unit based on PGO's JS16 USBDM-SWD design

with 4.12 Firmware) under Window 10 home editions OS and Codewarrior 5.1 for HCS12?

Any help will be very appreciated.

Thank you all.

 

USBDM-SWD

Labels (1)
0 Kudos
Reply
1 Solution
2,346 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Coti,

From the the CW 5.1 Release , we can see that the CW 5.1 not support the Win 10.

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,346 Views
ryanleis
Contributor I

is there anyway we can use USBDM on windows10? I know Microsoft sucks bigtime but we're needing help bad for our projects...!

0 Kudos
Reply
2,346 Views
RodneyMcGee
Contributor IV

Also use CW5.2 and add your missing devices using this

Add missing derivatives to CodeWarrior 5.2 (Unofficial Method)

CodeWarrior HCS12(X) 5.1 Windows 10 x64 Install and Update USBDM - YouTube

Check out this video, the steps are pretty much the same for 5.2.

0 Kudos
Reply
2,347 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Coti,

From the the CW 5.1 Release , we can see that the CW 5.1 not support the Win 10.

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply