Making the "Static Call Chart" file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Making the "Static Call Chart" file

2,097 次查看
etayluz
Contributor I
I would like a "Static Call Chart" HTML file to be created when I compile my *.mpc project. This is the HTML file that shows the flow of how functions call one another - it shows every function, which functions it calls, and which functions call on it. How do I enable this feature (I know that it exists). I have  ARM developer suite v1.2
标签 (1)
0 项奖励
回复
1 回复

1,022 次查看
CrasyCat
Specialist III
Hello
We do not have that available in CodeWarrior software.
However if you are using ARM developer suite v1.2, it may be an add-ons that ARM has developed and provides with the software.
 
I would recommend you to post a message on the ARM forum or to ARM support to get assistance.
 
CrasyCat
0 项奖励
回复