I was able to get the USB tap working with my target this morning by doing the following;
- Uninstall Codewarrior V8.0.
- Re-install Codewarrior V8.0.
- Connect the USB tap to the pc (prior to starting Codewarrior).
- Start Codewarrior.
The big difference this time is that the USB tap is now shown as a valid selection for the debug connection while it was not shown, and could not be selected, previously (before reinstall).
I did still need to edit ccs.cfg and change the "config cc parallel:2" to "config cc utap".
Everything is up and running now. Hope this helps someone out there.
Briang