For MC9S12DG256 chip, which Codewarrior?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For MC9S12DG256 chip, which Codewarrior?

1,222件の閲覧回数
lymantsinnie
Contributor I

Can't seem to get SE Codewarrior v5.2 to work with my Dragon12-plus2...I have found that this is not compatible...I'm lost. 

ラベル(1)
0 件の賞賛
返信
1 返信

1,041件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below thread

Which version of CodeWarrior for a MC9S12DG256 microcontroller? 

I hope this helps,

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信