For MC9S12DG256 chip, which Codewarrior?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For MC9S12DG256 chip, which Codewarrior?

1,245 Views
lymantsinnie
Contributor I

Can't seem to get SE Codewarrior v5.2 to work with my Dragon12-plus2...I have found that this is not compatible...I'm lost. 

Labels (1)
0 Kudos
Reply
1 Reply

1,064 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below thread

Which version of CodeWarrior for a MC9S12DG256 microcontroller? 

I hope this helps,

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply