Configurations are not remembered unless complete project is inside the default workspace directory.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Configurations are not remembered unless complete project is inside the default workspace directory.

912 次查看
davezawislak
Contributor II

When making different configurations off the same source, unless the complete project is inside the default workspace directory, only the original configuration is remembered. I have to recreate it if I leave CodeWarrior 10.2. It also does not save the "make this workspace the default" setting.

 

I have CW10.2 installed on Windows 7 in C:\Freescale.

标签 (1)
0 项奖励
回复
1 回复

773 次查看
J2MEJediMaster
Specialist I

You need to file  service request on this problem. Click here to go to the online service request page.

 

---Tom

0 项奖励
回复