Configurations are not remembered unless complete project is inside the default workspace directory.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configurations are not remembered unless complete project is inside the default workspace directory.

1,219件の閲覧回数
davezawislak
Contributor II

When making different configurations off the same source, unless the complete project is inside the default workspace directory, only the original configuration is remembered. I have to recreate it if I leave CodeWarrior 10.2. It also does not save the "make this workspace the default" setting.

 

I have CW10.2 installed on Windows 7 in C:\Freescale.

ラベル(1)
0 件の賞賛
返信
1 返信

1,080件の閲覧回数
J2MEJediMaster
Specialist I

You need to file  service request on this problem. Click here to go to the online service request page.

 

---Tom

0 件の賞賛
返信