smd microcontroller programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

smd microcontroller programming

Jump to solution
3,681 Views
wolfgangs
Fresh Out Contributor

Hello everyone.  I would like to know how surface mount Freescale micro-controllers are programmed.  Does Freescale offer to do this at the factory?  Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
2,396 Views
weapon
Senior Contributor I

Hi Wolfgang,

Generally speaking, regading MCU programing,  there're two cases:

1. MCU is mounted on PCB before programed. In such case, Programmers can use a cable to connect to BDM port (for S08 ) on the board to program MCUs.  P&E provides such kind of programmers, for example P&E Cyclone Pro

http://www.pemicro.com/products/product_processor.cfm?category=12

2. We also can program MCUs  directly by some dedicated programmers, there are one or more sockets in

the programmer, Put MCUs in them, one GUI in PC side can control the programming.

For example, Hilo System provides such kind of programmers

http://www.hilosystems.com.tw/en/hilo_products/programmer.aspx

Hope those information will be helpful.

View solution in original post

0 Kudos
Reply
1 Reply
2,397 Views
weapon
Senior Contributor I

Hi Wolfgang,

Generally speaking, regading MCU programing,  there're two cases:

1. MCU is mounted on PCB before programed. In such case, Programmers can use a cable to connect to BDM port (for S08 ) on the board to program MCUs.  P&E provides such kind of programmers, for example P&E Cyclone Pro

http://www.pemicro.com/products/product_processor.cfm?category=12

2. We also can program MCUs  directly by some dedicated programmers, there are one or more sockets in

the programmer, Put MCUs in them, one GUI in PC side can control the programming.

For example, Hilo System provides such kind of programmers

http://www.hilosystems.com.tw/en/hilo_products/programmer.aspx

Hope those information will be helpful.

0 Kudos
Reply