smd microcontroller programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

smd microcontroller programming

ソリューションへジャンプ
3,701件の閲覧回数
wolfgangs
Fresh Out Contributor

Hello everyone.  I would like to know how surface mount Freescale micro-controllers are programmed.  Does Freescale offer to do this at the factory?  Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,416件の閲覧回数
weapon
Senior Contributor I

Hi Wolfgang,

Generally speaking, regading MCU programing,  there're two cases:

1. MCU is mounted on PCB before programed. In such case, Programmers can use a cable to connect to BDM port (for S08 ) on the board to program MCUs.  P&E provides such kind of programmers, for example P&E Cyclone Pro

http://www.pemicro.com/products/product_processor.cfm?category=12

2. We also can program MCUs  directly by some dedicated programmers, there are one or more sockets in

the programmer, Put MCUs in them, one GUI in PC side can control the programming.

For example, Hilo System provides such kind of programmers

http://www.hilosystems.com.tw/en/hilo_products/programmer.aspx

Hope those information will be helpful.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,416件の閲覧回数
weapon
Senior Contributor I

Hi Wolfgang,

Generally speaking, regading MCU programing,  there're two cases:

1. MCU is mounted on PCB before programed. In such case, Programmers can use a cable to connect to BDM port (for S08 ) on the board to program MCUs.  P&E provides such kind of programmers, for example P&E Cyclone Pro

http://www.pemicro.com/products/product_processor.cfm?category=12

2. We also can program MCUs  directly by some dedicated programmers, there are one or more sockets in

the programmer, Put MCUs in them, one GUI in PC side can control the programming.

For example, Hilo System provides such kind of programmers

http://www.hilosystems.com.tw/en/hilo_products/programmer.aspx

Hope those information will be helpful.

0 件の賞賛
返信