smd microcontroller programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

smd microcontroller programming

跳至解决方案
3,650 次查看
wolfgangs
Contributor I

Hello everyone.  I would like to know how surface mount Freescale micro-controllers are programmed.  Does Freescale offer to do this at the factory?  Thanks.

标签 (1)
0 项奖励
回复
1 解答
2,365 次查看
weapon
Senior Contributor I

Hi Wolfgang,

Generally speaking, regading MCU programing,  there're two cases:

1. MCU is mounted on PCB before programed. In such case, Programmers can use a cable to connect to BDM port (for S08 ) on the board to program MCUs.  P&E provides such kind of programmers, for example P&E Cyclone Pro

http://www.pemicro.com/products/product_processor.cfm?category=12

2. We also can program MCUs  directly by some dedicated programmers, there are one or more sockets in

the programmer, Put MCUs in them, one GUI in PC side can control the programming.

For example, Hilo System provides such kind of programmers

http://www.hilosystems.com.tw/en/hilo_products/programmer.aspx

Hope those information will be helpful.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,366 次查看
weapon
Senior Contributor I

Hi Wolfgang,

Generally speaking, regading MCU programing,  there're two cases:

1. MCU is mounted on PCB before programed. In such case, Programmers can use a cable to connect to BDM port (for S08 ) on the board to program MCUs.  P&E provides such kind of programmers, for example P&E Cyclone Pro

http://www.pemicro.com/products/product_processor.cfm?category=12

2. We also can program MCUs  directly by some dedicated programmers, there are one or more sockets in

the programmer, Put MCUs in them, one GUI in PC side can control the programming.

For example, Hilo System provides such kind of programmers

http://www.hilosystems.com.tw/en/hilo_products/programmer.aspx

Hope those information will be helpful.

0 项奖励
回复