maximun voltage i/o digital for qe32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

maximun voltage i/o digital for qe32

1,182 Views
thinkchip
Contributor II

Hi, I want to know what is the maximum voltage for mc9s08qe32 for io digital, because I want to connect a lcd hd44780 and I dont know if could support the 5v,best regards

Labels (1)
0 Kudos
Reply
3 Replies

1,096 Views
bigmac
Specialist III

Hello,

 

You will need to operate the 'QE32 device from a 3.3 volt supply, and the LCD display from 5.0 volts.  However, assuming that the HD44780 is permanently set to write mode (as is often the case), the 3.3 volt swing from the MCU output pins should still be compatible with the switching threshold of the data and control inputs to the display.  Check this is true for the display you are using.

 

Regards,

Mac

 

0 Kudos
Reply

1,096 Views
RogerSchaefer
Contributor III

What bigmac said is true but there are a few LCDs that use  3.3 V

such as http://www.sparkfun.com/products/9054

 

 

Roger

0 Kudos
Reply

1,096 Views
Mickey
Contributor III

Absolute Maximum Ratings

Supply voltage VDD -0.3 to +3.8V

Digital input voltage VIN -0.3 to VDD+0.3

0 Kudos
Reply