maximun voltage i/o digital for qe32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

maximun voltage i/o digital for qe32

1,167 次查看
thinkchip
Contributor II

Hi, I want to know what is the maximum voltage for mc9s08qe32 for io digital, because I want to connect a lcd hd44780 and I dont know if could support the 5v,best regards

标签 (1)
0 项奖励
回复
3 回复数

1,081 次查看
bigmac
Specialist III

Hello,

 

You will need to operate the 'QE32 device from a 3.3 volt supply, and the LCD display from 5.0 volts.  However, assuming that the HD44780 is permanently set to write mode (as is often the case), the 3.3 volt swing from the MCU output pins should still be compatible with the switching threshold of the data and control inputs to the display.  Check this is true for the display you are using.

 

Regards,

Mac

 

0 项奖励
回复

1,081 次查看
RogerSchaefer
Contributor III

What bigmac said is true but there are a few LCDs that use  3.3 V

such as http://www.sparkfun.com/products/9054

 

 

Roger

0 项奖励
回复

1,081 次查看
Mickey
Contributor III

Absolute Maximum Ratings

Supply voltage VDD -0.3 to +3.8V

Digital input voltage VIN -0.3 to VDD+0.3

0 项奖励
回复