maximun voltage i/o digital for qe32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

maximun voltage i/o digital for qe32

1,239件の閲覧回数
thinkchip
Contributor II

Hi, I want to know what is the maximum voltage for mc9s08qe32 for io digital, because I want to connect a lcd hd44780 and I dont know if could support the 5v,best regards

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,153件の閲覧回数
bigmac
Specialist III

Hello,

 

You will need to operate the 'QE32 device from a 3.3 volt supply, and the LCD display from 5.0 volts.  However, assuming that the HD44780 is permanently set to write mode (as is often the case), the 3.3 volt swing from the MCU output pins should still be compatible with the switching threshold of the data and control inputs to the display.  Check this is true for the display you are using.

 

Regards,

Mac

 

0 件の賞賛
返信

1,153件の閲覧回数
RogerSchaefer
Contributor III

What bigmac said is true but there are a few LCDs that use  3.3 V

such as http://www.sparkfun.com/products/9054

 

 

Roger

0 件の賞賛
返信

1,153件の閲覧回数
Mickey
Contributor III

Absolute Maximum Ratings

Supply voltage VDD -0.3 to +3.8V

Digital input voltage VIN -0.3 to VDD+0.3

0 件の賞賛
返信