Why my sample project xBee doesn't compile ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why my sample project xBee doesn't compile ?

3,517件の閲覧回数
florianguillema
Contributor II

Hi,

 

I want to program on a xBee S2C module on CodeWarrior 10.2 and with the Programmable xBee SDK.

But I can't compile a sample project and I got that :

Invoking: HCS08 Compiler

"C:/Freescale/CW MCU v10.2/MCU/prog/chc08" -ArgFile"Sources/pan/zigbee/zigbee_zcl.args" -ObjN="Sources/pan/zigbee/zigbee_zcl_c.obj" "C:/Program Files/Digi/PXBee/v1.5/pxbee_api/1.5.5/src/pan/zigbee/zigbee_zcl.c" -Lm="Sources/pan/zigbee/zigbee_zcl_c.d" -LmCfg=xilmou

FATAL C50: Input file '-ObjN=Sources/pan/zigbee/zcl_client_c.obj' not found

I got this for a few files... I don't understand why cause I just followed this example :

Digi XBee® Examples & Guides | Step-by-step Tutorials for Implementing XBee® Wireless Modules in Ele...

 

Thanks for your help!

 

Regards

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,041件の閲覧回数
florianguillema
Contributor II

Today, I found the problem... I just found in renaming C:\CYGWIN in C:\CYGWIN-1 that the problem is solved.

Can anyone tell me a better solution than renaming the CYGWIN directory, please ?!?

Thanks!

3,041件の閲覧回数
florianguillema
Contributor II

Up please ^^

0 件の賞賛
返信

3,041件の閲覧回数
florianguillema
Contributor II

Oh and I get that for each file not found :

mingw32-make: *** [Sources/pan/zigbee/zcl_client_c.obj] Error 1

Hope it will be helpful ^^

0 件の賞賛
返信

3,041件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. CodeWarrior Development Tools or 8-bit Microcontrollers) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.