Simulations Work, Debug Fails: No source available for "0xFFFF (0xFFFF)() "

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simulations Work, Debug Fails: No source available for "0xFFFF (0xFFFF)() "

2,224 Views
yonathan
Contributor I

Hello,

I am using a MC9S08PL16 (CTJ) and codewarrior 11 (also tested on codewarrior 10.7). I have wrote a simple program to blink an LED. This program runs and performs successfully when testing in "Full Chip Simulation" but when testing on an actual unit the program turns on the LED but does not blink. 

When I try to debug the program I receive the error: No source available for "0xFFFF (0xFFFF)() " 

* Note: this error also happens when debugging a blank template program generated by codewarrior. 

When I look at the disassembly at 0xFFFF it shows: unable to retrieve disassembly data from backend

OxFFFF should host the reset interrupt vector which is properly defined. The setting up of the reset interrupt vector is defined by codewarrior and it looks correct.

Very similar to this problem: S08 Debug (Pause) No source available for "0xFFFF (0xFFFF)()" 

Please help me solve this problem!!!

Labels (1)
0 Kudos
Reply
1 Reply

2,053 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Yonathan

I already send you some samples on the internal case that you created

I hope this will help you.

0 Kudos
Reply