S08SG micro reset characteristics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08SG micro reset characteristics

1,217件の閲覧回数
pratikp1
Contributor I

I am working on the S08SG microcontroller. What is the effect on the state of the port pins if the Reset line is held low for a considerable duration of time (For e.g. if it is accidently short circuited to Ground). Also, does the micro keep resetting multiple times for the entire duration when the reset line is pulled to low(as it is a low level triggered reset) or it resets just once when the reset line goes high again?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,137件の閲覧回数
Stano
NXP Employee
NXP Employee

The reset line force the MCU pins to the high impedance when pulled low. The MCU will reset only once, when the reset lines goes high.

0 件の賞賛
返信