S08QG4, How to debug in STOP2/STOP1 mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08QG4, How to debug in STOP2/STOP1 mode?

ソリューションへジャンプ
1,476件の閲覧回数
w_tension
Contributor III

If the user attempts to enter either stop1 or stop2 with ENBDM set, the MCU will instead enter stop3.

As RM says. I can't actually enter stop2 when debug. Any suggestion? 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,300件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Yes this is correct if you have enable the BDM you only can enter to stop 3, you are not able to enter to stop 2 or 1 with the debugger enable.

regards

Vicente Gomez

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,301件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Yes this is correct if you have enable the BDM you only can enter to stop 3, you are not able to enter to stop 2 or 1 with the debugger enable.

regards

Vicente Gomez

0 件の賞賛
返信