S08QG4, How to debug in STOP2/STOP1 mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08QG4, How to debug in STOP2/STOP1 mode?

Jump to solution
1,594 Views
w_tension
Contributor III

If the user attempts to enter either stop1 or stop2 with ENBDM set, the MCU will instead enter stop3.

As RM says. I can't actually enter stop2 when debug. Any suggestion? 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,418 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Yes this is correct if you have enable the BDM you only can enter to stop 3, you are not able to enter to stop 2 or 1 with the debugger enable.

regards

Vicente Gomez

View solution in original post

0 Kudos
Reply
1 Reply
1,419 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Yes this is correct if you have enable the BDM you only can enter to stop 3, you are not able to enter to stop 2 or 1 with the debugger enable.

regards

Vicente Gomez

0 Kudos
Reply