S08QG4, How to debug in STOP2/STOP1 mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S08QG4, How to debug in STOP2/STOP1 mode?

跳至解决方案
1,045 次查看
w_tension
Contributor III

If the user attempts to enter either stop1 or stop2 with ENBDM set, the MCU will instead enter stop3.

As RM says. I can't actually enter stop2 when debug. Any suggestion? 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
869 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Yes this is correct if you have enable the BDM you only can enter to stop 3, you are not able to enter to stop 2 or 1 with the debugger enable.

regards

Vicente Gomez

在原帖中查看解决方案

0 项奖励
回复
1 回复
870 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Yes this is correct if you have enable the BDM you only can enter to stop 3, you are not able to enter to stop 2 or 1 with the debugger enable.

regards

Vicente Gomez

0 项奖励
回复