S08 SCI LBKD Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08 SCI LBKD Interrupt

1,246件の閲覧回数
qiongyu
Contributor I

I'm using S12 communicate with S08 via SCI。When S08 enable the break detect interrupt(set SCIxS2.LBKDE),no ISR reply. See the wave on RX pin with 13clk low, and in debug mode, the SCIxS2.LBKDIF is set. But can not jmp to the ISR.

 

When S08 disable the break detect inerrupt(clr SCIxS2.LBKDE),the S08 will jmp to ISR with receiver buffer full and Framing Error. I think the baud rate is the same as S12.

ラベル(1)
0 件の賞賛
返信
1 返信

1,085件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi, can you please tell me the device that you are using  (S08)

Thanks

Regards

Vicente Gomez

0 件の賞賛
返信