S08 SCI LBKD Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S08 SCI LBKD Interrupt

836 次查看
qiongyu
Contributor I

I'm using S12 communicate with S08 via SCI。When S08 enable the break detect interrupt(set SCIxS2.LBKDE),no ISR reply. See the wave on RX pin with 13clk low, and in debug mode, the SCIxS2.LBKDIF is set. But can not jmp to the ISR.

 

When S08 disable the break detect inerrupt(clr SCIxS2.LBKDE),the S08 will jmp to ISR with receiver buffer full and Framing Error. I think the baud rate is the same as S12.

标签 (1)
0 项奖励
回复
1 回复

675 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi, can you please tell me the device that you are using  (S08)

Thanks

Regards

Vicente Gomez

0 项奖励
回复