LVD Detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,398件の閲覧回数
chetan
Contributor I

i want to know how to generate LVD interrupt from bean inspector in  MC9S08PT16

ラベル(1)
タグ(4)
1 解決策
2,249件の閲覧回数
arpitaagarwal-b
NXP Employee
NXP Employee

Hello Chetan,

LVD Interrupt can be enabled in CPU bean (once the PE is enabled in the project, no need to add any other bean) from the options available in component inspector. To see the list of the options switch to "Expert" view (circled in the image below) of the inspector. Go to Internal Peripherals-->LVD Module-->LVW interrupt to enable the interrupt.

LVD_PT16.png

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,250件の閲覧回数
arpitaagarwal-b
NXP Employee
NXP Employee

Hello Chetan,

LVD Interrupt can be enabled in CPU bean (once the PE is enabled in the project, no need to add any other bean) from the options available in component inspector. To see the list of the options switch to "Expert" view (circled in the image below) of the inspector. Go to Internal Peripherals-->LVD Module-->LVW interrupt to enable the interrupt.

LVD_PT16.png

0 件の賞賛
返信
2,249件の閲覧回数
chetan
Contributor I

Dear Arpita

Thanks a lot arpita

Problem solved I don’t know to see it in "Expert" view

Best Regards,

Chetan Namjoshi

2,249件の閲覧回数
Monica
Senior Contributor III

Hello Chetan!

I ran into this document, maybe it has the info you need MC9S08PT16 Reference Manual

Hope it helps!

Regards,

Monica.

0 件の賞賛
返信