LVD Detection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LVD Detection

跳至解决方案
1,546 次查看
chetan
Contributor I

i want to know how to generate LVD interrupt from bean inspector in  MC9S08PT16

标签 (1)
标记 (4)
1 解答
1,397 次查看
arpitaagarwal-b
NXP Employee
NXP Employee

Hello Chetan,

LVD Interrupt can be enabled in CPU bean (once the PE is enabled in the project, no need to add any other bean) from the options available in component inspector. To see the list of the options switch to "Expert" view (circled in the image below) of the inspector. Go to Internal Peripherals-->LVD Module-->LVW interrupt to enable the interrupt.

LVD_PT16.png

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,398 次查看
arpitaagarwal-b
NXP Employee
NXP Employee

Hello Chetan,

LVD Interrupt can be enabled in CPU bean (once the PE is enabled in the project, no need to add any other bean) from the options available in component inspector. To see the list of the options switch to "Expert" view (circled in the image below) of the inspector. Go to Internal Peripherals-->LVD Module-->LVW interrupt to enable the interrupt.

LVD_PT16.png

0 项奖励
回复
1,397 次查看
chetan
Contributor I

Dear Arpita

Thanks a lot arpita

Problem solved I don’t know to see it in "Expert" view

Best Regards,

Chetan Namjoshi

1,397 次查看
Monica
Senior Contributor III

Hello Chetan!

I ran into this document, maybe it has the info you need MC9S08PT16 Reference Manual

Hope it helps!

Regards,

Monica.

0 项奖励
回复