How to create a project including two targets in CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to create a project including two targets in CodeWarrior

2,702 Views
baonguyen
Contributor I
Dear everybody,

I want to creat a project including two targets in Metrowerk's CodeWarrior. How to do that? How to associate the code corresponding with each target ?

Thanks in advance,
Best regards
Labels (1)
0 Kudos
Reply
1 Reply

1,476 Views
fire
Contributor I

it's simple.

Click on target menu.

Choose one target.

go to project-->Create target.

here you can clone the target or create a new target.

if you are cloning you have to change the name twice in target settings.

then add the files required for the target.

you can remove the files from any target using project inspector.

Regards,

Fire

 

 

0 Kudos
Reply