How to create a project including two targets in CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to create a project including two targets in CodeWarrior

2,738件の閲覧回数
baonguyen
Contributor I
Dear everybody,

I want to creat a project including two targets in Metrowerk's CodeWarrior. How to do that? How to associate the code corresponding with each target ?

Thanks in advance,
Best regards
ラベル(1)
0 件の賞賛
返信
1 返信

1,512件の閲覧回数
fire
Contributor I

it's simple.

Click on target menu.

Choose one target.

go to project-->Create target.

here you can clone the target or create a new target.

if you are cloning you have to change the name twice in target settings.

then add the files required for the target.

you can remove the files from any target using project inspector.

Regards,

Fire

 

 

0 件の賞賛
返信