External Crystal = 32 kHz, Maximum bus Frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External Crystal = 32 kHz, Maximum bus Frequency

ソリューションへジャンプ
2,667件の閲覧回数
WillemEradus
Contributor I

 

I have an evolution board with a MC9S08LC60 and an external crystal of 32 kHz. In the example, the FLL will be used (in FEE mode) to multiply the external 32 kHz oscillator up to 8.38MHz to achieve 4.19 MHz bus frequency.  My question is what is the maximum bus frequency I can achieve with this setup.

 

Thx, Willem. 


ラベル(1)
0 件の賞賛
返信
1 解決策
1,641件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora, Willem.

 

In your example the multiplier used is 4.

The maximum multiplier available is 18

4.19 * 18 / 4 = 18.8MHz

 

Refer to datasheet Chapter 10, ICG for more details .

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,642件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora, Willem.

 

In your example the multiplier used is 4.

The maximum multiplier available is 18

4.19 * 18 / 4 = 18.8MHz

 

Refer to datasheet Chapter 10, ICG for more details .

 

0 件の賞賛
返信
1,641件の閲覧回数
WillemEradus
Contributor I
thanks !
0 件の賞賛
返信