External Crystal = 32 kHz, Maximum bus Frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

External Crystal = 32 kHz, Maximum bus Frequency

跳至解决方案
2,683 次查看
WillemEradus
Contributor I

 

I have an evolution board with a MC9S08LC60 and an external crystal of 32 kHz. In the example, the FLL will be used (in FEE mode) to multiply the external 32 kHz oscillator up to 8.38MHz to achieve 4.19 MHz bus frequency.  My question is what is the maximum bus frequency I can achieve with this setup.

 

Thx, Willem. 


标签 (1)
0 项奖励
回复
1 解答
1,657 次查看
peg
Senior Contributor IV

Hello and welcome to the fora, Willem.

 

In your example the multiplier used is 4.

The maximum multiplier available is 18

4.19 * 18 / 4 = 18.8MHz

 

Refer to datasheet Chapter 10, ICG for more details .

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,658 次查看
peg
Senior Contributor IV

Hello and welcome to the fora, Willem.

 

In your example the multiplier used is 4.

The maximum multiplier available is 18

4.19 * 18 / 4 = 18.8MHz

 

Refer to datasheet Chapter 10, ICG for more details .

 

0 项奖励
回复
1,657 次查看
WillemEradus
Contributor I
thanks !
0 项奖励
回复