External Crystal = 32 kHz, Maximum bus Frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External Crystal = 32 kHz, Maximum bus Frequency

Jump to solution
2,691 Views
WillemEradus
Contributor I

 

I have an evolution board with a MC9S08LC60 and an external crystal of 32 kHz. In the example, the FLL will be used (in FEE mode) to multiply the external 32 kHz oscillator up to 8.38MHz to achieve 4.19 MHz bus frequency.  My question is what is the maximum bus frequency I can achieve with this setup.

 

Thx, Willem. 


Labels (1)
0 Kudos
Reply
1 Solution
1,665 Views
peg
Senior Contributor IV

Hello and welcome to the fora, Willem.

 

In your example the multiplier used is 4.

The maximum multiplier available is 18

4.19 * 18 / 4 = 18.8MHz

 

Refer to datasheet Chapter 10, ICG for more details .

 

View solution in original post

0 Kudos
Reply
2 Replies
1,666 Views
peg
Senior Contributor IV

Hello and welcome to the fora, Willem.

 

In your example the multiplier used is 4.

The maximum multiplier available is 18

4.19 * 18 / 4 = 18.8MHz

 

Refer to datasheet Chapter 10, ICG for more details .

 

0 Kudos
Reply
1,665 Views
WillemEradus
Contributor I
thanks !
0 Kudos
Reply