802.15.4 MAC-2006 Realignment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

802.15.4 MAC-2006 Realignment

1,124 次查看
hein
Contributor I

Hello All,

 

I use the Freescale 802.15.4 MAC-2006 at MC13213.

 

The Coordinator will perform a channel change and sends a realignment with the new channel (tested using RF Sniffer). The device receives the realignment and triggers a MLME-Msg: Sync.loss-Indication with Reason "realignment" correct.

 

The parameter “Logical Channel field” shall contain the logical channel that the coordinator intends to use for all future communications, but this parameter is the „old“ channel and so the device does not change the channel.

 

The MAC does not assume the channel. The channel change fails.

 

What can I do?

 

Regards

Hein

标签 (1)
0 项奖励
回复
2 回复数

800 次查看
hein
Contributor I

Hello,

 

ist there no one who has an idea?

Is this a bug in the MAC, or an error in my implementation?

 

Regards

Hein

0 项奖励
回复

800 次查看
J2MEJediMaster
Specialist I

You should file a service request on that. Click here to file an on-line service request.

 

---Tom

0 项奖励
回复