802.15.4 MAC-2006 Realignment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

802.15.4 MAC-2006 Realignment

1,705件の閲覧回数
hein
Contributor I

Hello All,

 

I use the Freescale 802.15.4 MAC-2006 at MC13213.

 

The Coordinator will perform a channel change and sends a realignment with the new channel (tested using RF Sniffer). The device receives the realignment and triggers a MLME-Msg: Sync.loss-Indication with Reason "realignment" correct.

 

The parameter “Logical Channel field” shall contain the logical channel that the coordinator intends to use for all future communications, but this parameter is the „old“ channel and so the device does not change the channel.

 

The MAC does not assume the channel. The channel change fails.

 

What can I do?

 

Regards

Hein

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,381件の閲覧回数
hein
Contributor I

Hello,

 

ist there no one who has an idea?

Is this a bug in the MAC, or an error in my implementation?

 

Regards

Hein

0 件の賞賛
返信

1,381件の閲覧回数
J2MEJediMaster
Specialist I

You should file a service request on that. Click here to file an on-line service request.

 

---Tom

0 件の賞賛
返信