iMX6 TW686x Surround view patch

Document created by Justin Jiang Employee on Jul 17, 2013Last modified by Adrian Puga Candelario on Jan 9, 2019
Version 8Show Document
  • View in full screen mode

We use PCIe to connect Intersil TW6865 chip for the surround view solution.

This is the connection of PCIe to iMX6Q SabreSD board.1.JPG

 

This is the block diagram of the connection:

3.JPG

This is the 4 camera surround view:4.JPG

 

Code base is L3.0.35_12.10.02 release. You can merge the patch file to the latest Freescale release.

Please check the attach file for the patch code.

 

Note:  It is only a test version.

Original Attachment has been moved to: pcie_cap_patch.patch.zip

 

The last code for L3.0.35 BSP: L3.0.35_GA4.1.0 Patches.7z

The last code for L3.10.53 BSP: L3.10.53_TW686x_patch.7z

Patch for L4.1.15 1.1.0 GA BSP: TW6865 driver for Linux L4.1.15_1.1.0-ga.7z

10 people found this helpful

Outcomes