i.MX Yocto Project: How Can I Build the Freescale Yocto Images using bitbake?

Document created by Leonardo Sandoval Gonzalez Employee on Jan 29, 2013Last modified by Leonardo Sandoval Gonzalez Employee on Jun 12, 2013
Version 7Show Document
  • View in full screen mode

1. Follow all steps from Freescale's github repo except the last bitbake command

2. The images that Freescale supports are located on the meta-fsl-demos/recipes-fsl/images folder.

3. Bake the standard Freescale image

build$ bitbake fsl-image-gui

 

4. The produced Linux image is packaged in several formats; the .sdcard single file has all the system (u-boot + uImage + rootfs) so it can be directly flashed into an SD card

build$ sudo dd if=tmp/deploy/images/fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=4M

NOTES:

  • In case of building issues, please follow this link
  • In case of booting issues, make sure: 1. board DIP switches are set correctly 2. you have chosen the correct machine before baking
  • If issues persist, report it to the community


1 person found this helpful

Attachments

    Outcomes