1. Follow all steps from Freescale's github repo except the last bitbake command
2. The images that Freescale supports are located on the meta-fsl-demos/recipes-fsl/images folder.
3. Bake the standard Freescale image
build$ bitbake fsl-image-gui
4. The produced Linux image is packaged in several formats; the .sdcard single file has all the system (u-boot + uImage + rootfs) so it can be directly flashed into an SD card
build$ sudo dd if=tmp/deploy/images/fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=4M
NOTES:
How can I add Kernel Support for Flexcan?
I am not sure. Please ask this question into the Yocto Project mailing list.
Hi,
May I ask a question about this process? I followed the instructions above as far as '$ repo sync' and this fails with a bunch of messages along the lines of:
fatal: unable to connect to github.com:
github.com[0: 204.232.175.90]: errno=Connection timed out
and eventually gives up with:
error: Exited sync due to fetch errors
I am behind a proxy, so suspecting this is the problem I read and followed the instructions here: https://wiki.yoctoproject.org/wiki/Working_Behind_a_Network_Proxy using the socat method. The '$ repo sync' step still fails but with slightly different results, now I get messages of the sort:
2013/06/19 11:37:59 socat[9115] E getaddrinfo("", "(null)", {1,0,1,6}, {}): No such file or directory
2013/06/19 11:37:59 socat[9114] E getaddrinfo("", "(null)", {1,0,1,6}, {}): No such file or directory
2013/06/19 11:37:59 socat[9113] E getaddrinfo("", "(null)", {1,0,1,6}, {}): No such file or directory
fatal: Could not read from remote repository.
Please make sure you have the correct access rights
and the repository exists.
fatal: Could not read from remote repository.
Any ideas would be most welcome.
Cheers,
John.
I think you are missing 'socat' utility.
$: sudo apt-get install socat
Hello,
Thank you very much for your reply. However, I had already done this, witness:
$ socat -V
socat by Gerhard Rieger - see www.dest-unreach.org
socat version 1.7.1.3 on Jul 21 2012 00:02:19
running on Linux version #29-Ubuntu SMP Wed Apr 17 18:19:42 UTC 2013, release 3.8.0-19-generic, machine i686
features:
...
I also tried the nc method from the page that I linked to before. This also failed with these errors of this form:
nc: read failed (0/8): Connection reset by peer
fatal: Could not read from remote repository.
Please make sure you have the correct access rights
and the repository exists.
Do I need access rights? Or do you think this is also a proxy issue? If so, what else am I missing to get through the proxy?
Again, thanks for your help.
Cheers,
John.
I'd try to check if GIT is really using the proxy script; maybe using a strace or something to debug it.
As I am not a proxy user, I cannot be of much help but maybe you could ask in openembedded-users mailing list about it?
Sorry but I couldn't understand you properly.
Have you succeed ?
I'm a bit new to this but is this instruction still valid?
I followed the instructions but when I get to the "build$ bitbake fsl-image-gui" step it will process for a while and then:
ERROR: Nothing PROVIDES 'fsl-image-gui'. Close matches:
fsl-image-multimedia
I'm now running
build$ bitbake fsl-image-multimedia
Hi
David
You can use following command to verify supported images
bitbake-layers show-recipes | grep image
Thanks
Saurabh
Hi
David
You can refer "Freescale_Yocto_project_user's_guide.pdf"
SABRE Board Reference Design|Freescale
You can download 'L3.14.28_1.0.0_LINUX_DOCS" or L3.10.53_1.1.0_LINUX_DOCS 
Where can i find the libsub for ultra light board??
Hi,
Is it possible to build freescale yocto images using eclipse ? If so anyone knows steps for the same?
Thank You,
Sharmila