S32 Design Studio for Power v1.2 (Windows/Linux) released!

Document created by stanish Employee on Jun 19, 2017Last modified by stanish Employee on Jun 22, 2017
Version 2Show Document
  • View in full screen mode





Product Release Announcement

Automotive Microcontrollers and Processors

S32 Design Studio for Power v1.2







S32 Design Studio for Power v1.2 (Windows/Linux) has been released. This is a complete installer which does not require any previous version to be installed.


To download the installer please visit download section: www.nxp.com/s32ds



What is new?


New devices:

• MPC5632M, MPC5633M, MPC5634M
• MPC5642A
• MPC5674F
• MPC5673K, MPC5674K, MPC5675K
• S32R372

New features:

• Compiler update – see details in compiler release notes attached below
• View for the Special Purpose Registers added
• Improvements for Peripherals Register view
• Added support for Semihosting/Debug console for single core devices
• RESET functionality added, the hardware reset2 is executed for main/boot core and individual core reset for secondary cores.
• Improvements for SPT diagram to display instruction labels and key parameters
• SDK mechanism improvements to support SDK per build configuration
• FreeMaster Serial Communication driver 2.0 integrated
• iSystem debugger support added to New Project Wizard
• SPT assembler update
• Updated P&E debug plugins and drivers to the latest and greatest versions


The plugins to support GreenHills, IAR, iSystem, Lauterbach are not included and have to be installed from corresponding update site or installation.


S32DS release notes are available here.

GCC Build tools release notes are here.


Installation Notes

The installer requires NEW Activation ID to be entered during the installation. You should receive an email including the Activation ID after starting the download process e.g:




2 people found this helpful