Sensors software examples published by NXP technical support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensors software examples published by NXP technical support

Sensors software examples published by NXP technical support

FRDM-STBC-AGM01: 9-Axis Inertial Measurement Sensor Board

FRDM-KL25Z FRDM-STBC-AGM01 - Example project in KDS 3.0.0 using KSDK 1.2.0 and Processor Expert

FRDM-STBC-AGM01 - Bare metal example project

 

FRDMSTBC-A8471: 3-Axis Accelerometer Sensor Toolbox Development Board

FRDMSTBC-A8471 - Bare metal example project

FRDMSTBC-A8471 - Example project in KDS 3.0.2 using KSDK 2.0

FXLS8471Q Auto-sleep with Transient threshold trigger 

 

MPL3115A2: 20 to 110kPa, Absolute Digital (I2C) Pressure Sensor

MPL3115A2 - Bare metal example project

FRDMKL25-P3115 - Example project in KDS 3.0.2 using KSDK 2.0

https://community.nxp.com/docs/DOC-345632 

 

MPL115A1: 50 to 115kPa, Absolute Digital (SPI) Pressure Sensor

MPL115A1- Bare metal example project 

 

FXOS8700CQ: Digital (I2C/SPI) Sensor - 3-Axis Accelerometer (±2g/±4g/±8g) + 3-Axis Magnetometer

FXOS8700CQ - Bare metal example project

FXOS8700CQ - Magnetic threshold detection function example code 

FXOS8700CQ - Auto-sleep with Magnetic threshold trigger 

 

FXLS8471Q: ±2g/±4g/±8g, 3-Axis, 14-Bit Digital (I2C/SPI) Accelerometer

FXLS8471Q - Bare metal example project

FXLS8471Q - FIFO Fill mode example code

FXLS8471Q - Accelerometer vector-magnitude function example code

FXLS8471Q - Accelerometer transient detection function example code

FXLS8471Q - Accelerometer motion detection function example code 

FXLS8471Q - Accelerometer orientation detection function example code 

 

MMA8652FC: ±2g/±4g/±8g, 3-Axis, 12-Bit Digital (I2C) Accelerometer

MMA8652FC - Bare metal example project

MMA8652FC - Auto-WAKE/SLEEP mode

 

MMA8451Q: ±2g/±4g/±8g, 3-Axis, 14-bit Digital (I2C) Accelerometer

MMA8451Q - Bare metal example project

MMA8451Q - Single Tap Detection Bare metal example project

FRDM-KL27Z MMA8451Q - How to build and run an ISSDK based example project 

 

MMA8491Q: ±8g, 3-Axis, 14-bit Digital (I2C) Accelerometer/Tilt Sensor

MMA8491Q - Acceleration data streaming using the PIT on the Kinetis KL25Z MCU

 

FXLN83xxQ: 3-Axis, Low-Power, Analog Accelerometer

FXLN8371Q - Bare metal example project

 

FXAS21002C: 3-Axis Digital (I2C/SPI) Gyroscope

FXAS21000 – Bare metal example project

FXAS21002C - Angular rate threshold detection function example code

 

MAG3110FC: 3-Axis Digital (I2C) Magnetometer

MAG3110FC – Bare metal example project

 

LM75A: Digital temperature sensor and thermal watchdog

LM75A - Temperature data streaming using the PIT on the Kinetis KL25Z MCU

Comments

Dear, I need a sensor that performs pressure measurement of liquefied petroleum gas (cooking gas) in Brazil Pressure range 300 kpa up to 700kpa What is the sensor? Who can help me ?

No ratings
Version history
Last update:
‎02-03-2026 05:11 PM
Updated by: