FRDM-STBC-AGM01: 9-Axis Inertial Measurement Sensor Board
FRDM-KL25Z FRDM-STBC-AGM01 - Example project in KDS 3.0.0 using KSDK 1.2.0 and Processor Expert
FRDM-STBC-AGM01 - Bare metal example project
FRDMSTBC-A8471: 3-Axis Accelerometer Sensor Toolbox Development Board
FRDMSTBC-A8471 - Bare metal example project
FRDMSTBC-A8471 - Example project in KDS 3.0.2 using KSDK 2.0
FXLS8471Q Auto-sleep with Transient threshold trigger
MPL3115A2: 20 to 110kPa, Absolute Digital (I2C) Pressure Sensor
MPL3115A2 - Bare metal example project
FRDMKL25-P3115 - Example project in KDS 3.0.2 using KSDK 2.0
https://community.nxp.com/docs/DOC-345632
MPL115A1: 50 to 115kPa, Absolute Digital (SPI) Pressure Sensor
MPL115A1- Bare metal example project
FXOS8700CQ: Digital (I2C/SPI) Sensor - 3-Axis Accelerometer (±2g/±4g/±8g) + 3-Axis Magnetometer
FXOS8700CQ - Bare metal example project
FXOS8700CQ - Magnetic threshold detection function example code
FXOS8700CQ - Auto-sleep with Magnetic threshold trigger
FXLS8471Q: ±2g/±4g/±8g, 3-Axis, 14-Bit Digital (I2C/SPI) Accelerometer
FXLS8471Q - Bare metal example project
FXLS8471Q - FIFO Fill mode example code
FXLS8471Q - Accelerometer vector-magnitude function example code
FXLS8471Q - Accelerometer transient detection function example code
FXLS8471Q - Accelerometer motion detection function example code
FXLS8471Q - Accelerometer orientation detection function example code
MMA8652FC: ±2g/±4g/±8g, 3-Axis, 12-Bit Digital (I2C) Accelerometer
MMA8652FC - Bare metal example project
MMA8652FC - Auto-WAKE/SLEEP mode
MMA8451Q: ±2g/±4g/±8g, 3-Axis, 14-bit Digital (I2C) Accelerometer
MMA8451Q - Bare metal example project
MMA8451Q - Single Tap Detection Bare metal example project
FRDM-KL27Z MMA8451Q - How to build and run an ISSDK based example project
MMA8491Q: ±8g, 3-Axis, 14-bit Digital (I2C) Accelerometer/Tilt Sensor
MMA8491Q - Acceleration data streaming using the PIT on the Kinetis KL25Z MCU
FXLN83xxQ: 3-Axis, Low-Power, Analog Accelerometer
FXLN8371Q - Bare metal example project
FXAS21002C: 3-Axis Digital (I2C/SPI) Gyroscope
FXAS21000 – Bare metal example project
FXAS21002C - Angular rate threshold detection function example code
MAG3110FC: 3-Axis Digital (I2C) Magnetometer
MAG3110FC – Bare metal example project
LM75A: Digital temperature sensor and thermal watchdog
LM75A - Temperature data streaming using the PIT on the Kinetis KL25Z MCU
Dear, I need a sensor that performs pressure measurement of liquefied petroleum gas (cooking gas) in Brazil Pressure range 300 kpa up to 700kpa What is the sensor? Who can help me ?