As of February 2, 2026, the NXP MEMS Sensor products have been transferred to STMicroelectronics. For details on the transferred products, see this page. Please reach out to STMicroelectronics for further information.
*************************************************************************************************************
* This simple example code has been written for the NXP FRDM-KL25Z + FRDMSTBC-A8471
* boards and demonstrates how to use the embedded transient detection function
* in conjunction with the auto-wake/sleep mode for reducing current consumption
* of the FXLS8471Q.
*
* The transient threshold is set to 312.5mg (5 counts) on the X and Y axis.
* Once this threshold is exceeded, the FXLS8471Q is waken up and an interrupt
* is generated on the INT1 pin. If the acceleration is below this threshold
* within the 1s period, the FXLS8471Q goes back to sleep mode and also
* generates an interrupt on the INT1 pin.
*************************************************************************************************************