How to add drivers to MCUexpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add drivers to MCUexpresso

Jump to solution
11,125 Views
randylee
Contributor V

I'm using MCUexpresso 10.2 with SDK 2.4

When you create a project, it asks all kinds of things including what drivers you want in it, which is fine.

The problem I'm having is that I need to add some drivers into the project.  I can't figure out how to do that at this point. 

How do I edit the list of drivers and middleware that was originally used to generate the project as the project evolves?

In KDS and PEX this is trivial to do.....

Tags (2)
0 Kudos
Reply
1 Solution
9,857 Views
BlackNight
NXP Employee
NXP Employee

Hi Randy,

there is a button to add/remove SDK drivers/components. See Eclipse MCUXpresso IDE 10.1 with integrated MCUXpresso Configuration Tools | MCU on Eclipse  and search for "add/remove components".

I hope this helps,

Erich

View solution in original post

2 Replies
9,858 Views
BlackNight
NXP Employee
NXP Employee

Hi Randy,

there is a button to add/remove SDK drivers/components. See Eclipse MCUXpresso IDE 10.1 with integrated MCUXpresso Configuration Tools | MCU on Eclipse  and search for "add/remove components".

I hope this helps,

Erich

9,857 Views
randylee
Contributor V

yes indeed, that's it....  Saved again. Thanx much!

0 Kudos
Reply