How to add drivers to MCUexpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to add drivers to MCUexpresso

跳至解决方案
9,859 次查看
randylee
Contributor V

I'm using MCUexpresso 10.2 with SDK 2.4

When you create a project, it asks all kinds of things including what drivers you want in it, which is fine.

The problem I'm having is that I need to add some drivers into the project.  I can't figure out how to do that at this point. 

How do I edit the list of drivers and middleware that was originally used to generate the project as the project evolves?

In KDS and PEX this is trivial to do.....

标记 (2)
0 项奖励
回复
1 解答
8,591 次查看
BlackNight
NXP Employee
NXP Employee

Hi Randy,

there is a button to add/remove SDK drivers/components. See Eclipse MCUXpresso IDE 10.1 with integrated MCUXpresso Configuration Tools | MCU on Eclipse  and search for "add/remove components".

I hope this helps,

Erich

在原帖中查看解决方案

2 回复数
8,592 次查看
BlackNight
NXP Employee
NXP Employee

Hi Randy,

there is a button to add/remove SDK drivers/components. See Eclipse MCUXpresso IDE 10.1 with integrated MCUXpresso Configuration Tools | MCU on Eclipse  and search for "add/remove components".

I hope this helps,

Erich

8,591 次查看
randylee
Contributor V

yes indeed, that's it....  Saved again. Thanx much!

0 项奖励
回复