i.MX7/PF3000 RTC Backup Power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7/PF3000 RTC Backup Power

Jump to solution
3,062 Views
demoniacmilk
Contributor IV

Hello Community,

I am wondering about the RTC section of the i.MX7 and power supply in combination with a PF3000 PMIC and if I understood everything correctly.
Based on this I want to decide wether the i.MX7 internal RTC is suited or if an external RTC is the way to go.

The PF3000 / i.MX7 provide NVCC voltage rails for e.g. the RTC. These allow power states with most of the system disabled, including many power rails, clocks, cores etc. If the systems power is cut the NVCC voltage rails should not be powered anymore. Some kind of backup power supply for the RTC is needed.

On pin 36 (LICELL) a Lithium Cell may be connected to the system. The PF3000 provides an internal LiCell charger. Registers allow to enable/disable the charger and to set the batterys/caps voltage. All SNVS regions are powered by either an internal LDO (if the systems input voltage is above a certain threshold) or the battery.

Coin cell power mode (all power rails etc turned off) current consumption: up to 7uA based on '5.3 - current consumption' in the PF3000 datasheet. This is probably the current consumption of the PF3000 itsself?
It is said the current will increase when the voltage drops, up to 50uA. Are there any graphs or additional info on how the current increases?

I cannot find information on the i.MX7D current consumption when only the SNVS rails are powered. Only information I could find is in another thread: NXP Community 

Based on this, around 500uA at 3V are consume. For a 4 Month backup (from PCB manufacturing until system delivery), assuming constant voltage and current, a 1.4 Ah battery is necessary, (without self discharge) (correct?).
As an alternative, a supercap storing 1.4Ah*3V = 4,2 Wh = 15 kWs could be used. For a voltage drop of 2V7 .. 1V8, this means a 7500F capacitor (!!!) is required, so a capacitor is out of question. Or did I miscalculate here?

Dedicated RTCs require about 50nA supply current, what is just 1/10000 of the mx7 requirement. I should certainly go with a dedicated RTC, if the assumptions above are correct and if the mx7 + pf3000 RTC power backup really consumes about 500uA continously when powered off.

Labels (3)
0 Kudos
Reply
1 Solution
2,426 Views
Yuri
NXP Employee
NXP Employee

Hello,

  In general Your considerations are correct. Note, according to  i.MX7D Datasheet :
SNVS mode is also called RTC mode, where only the power for the SNVS domain remain on.

In this mode, only the RTC and tamper detection logic is still active. The power consumption in SNVS

mode with all the tamper detection logic enabled will be less than 5 uA @ 3.0 V on VDD_SNVS_IN for typical

silicon at 25°C.

  External RTC may be preferable solution when it is needed to get coin cell based power during

long time. It is very hard to create RTC with nA consumption as part of a SOC.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,426 Views
Yuri
NXP Employee
NXP Employee

Hello,

  In general Your considerations are correct. Note, according to  i.MX7D Datasheet :
SNVS mode is also called RTC mode, where only the power for the SNVS domain remain on.

In this mode, only the RTC and tamper detection logic is still active. The power consumption in SNVS

mode with all the tamper detection logic enabled will be less than 5 uA @ 3.0 V on VDD_SNVS_IN for typical

silicon at 25°C.

  External RTC may be preferable solution when it is needed to get coin cell based power during

long time. It is very hard to create RTC with nA consumption as part of a SOC.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply