question about imx6 pcie's frequency/clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question about imx6 pcie's frequency/clock

Jump to solution
2,566 Views
jiangyaqiang
Senior Contributor I

                                                                                 question about imx6 pcie's clock

      In the document of "reference manual", there are three source clocks for  phy_ref_output_clk, but how to select it ?

Refer as bellow:

pastedImage_1.png

linux version: 4.1.15

Labels (5)
0 Kudos
Reply
1 Solution
2,023 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiang

by default 125MHz is used in imx6qdl.dtsi :

clks IMX6QDL_CLK_PCIE_REF_125M

linux-imx.git - i.MX Linux Kernel 

also other clocks may be selected as described on

IMX6 PCI with external clocks  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,024 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiang

by default 125MHz is used in imx6qdl.dtsi :

clks IMX6QDL_CLK_PCIE_REF_125M

linux-imx.git - i.MX Linux Kernel 

also other clocks may be selected as described on

IMX6 PCI with external clocks  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply