(
converted from discussion created by Alfred Latypov
)
Hello, I had a problem, to launch a board with an imx6 solo processor with a pci-express, and with external clock. I'll tell you my decision.
On my motherboard there is a pci-switch PI7C9X2G606 from Pericom with 4 endpoints of Intel type 82574 ethernet controller.
I used the Linux kernel version 4.9.16
In the device-tree file, I used the following options to enable external clocks for CLK1 input gate (100MHz). Sorry, I had to change the root imx6 device tree file. See attached (imx6*.dtsi) files. From ..kernel/arch/arm/boot/dts/..
Add anatop external clock source for clocks section, and change clk source for pcie-phy.
...
anaclk1 {
compatible = "fixed-clock";
reg = <0>;
#clock-cells = <0>;
clock-frequency = <100000000>; /* 100MHz */
};
...
Change pcie section
...
pcie: pcie@0x01000000 {
compatible = "fsl,imx6q-pcie", "snps,dw-pcie";
reg = <0x01ffc000 0x04000>,
<0x01f00000 0x80000>;
reg-names = "dbi", "config";
#address-cells = <3>;
#size-cells = <2>;
device_type = "pci";
ranges = <0x81000000 0 0 0x01e00000 0 0x00100000 /* downstream I/O */
0x82000000 0 0x01000000 0x01000000 0 0x00e00000>; /* non-prefetchable memory */
/* ranges = <0x81000000 0 0 0x01f80000 0 0x00010000
0x82000000 0 0x01000000 0x01000000 0 0x00f00000>; */
num-lanes = <1>;
interrupts = <GIC_SPI 120 IRQ_TYPE_LEVEL_HIGH>;
interrupt-names = "msi";
#interrupt-cells = <1>;
interrupt-map-mask = <0 0 0 0x7>;
interrupt-map = <0 0 0 1 &gpc GIC_SPI 123 IRQ_TYPE_LEVEL_HIGH>,
<0 0 0 2 &gpc GIC_SPI 122 IRQ_TYPE_LEVEL_HIGH>,
<0 0 0 3 &gpc GIC_SPI 121 IRQ_TYPE_LEVEL_HIGH>,
<0 0 0 4 &gpc GIC_SPI 120 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6QDL_CLK_PCIE_AXI>,
<&clks IMX6QDL_CLK_LVDS1_IN>,
<&clks IMX6QDL_CLK_SATA_REF_100M>;
clock-names = "pcie", "pcie_bus", "pcie_phy";
status = "disabled";
};
...
and add new source clocks dependencies:
....
&clks {
assigned-clocks = <&clks IMX6QDL_PLL6_BYPASS_SRC>,
<&clks IMX6QDL_PLL6_BYPASS>;
assigned-clock-parents = <&clks IMX6QDL_CLK_LVDS1_IN>,
<&clks IMX6QDL_PLL6_BYPASS_SRC>;
assigned-clock-rates = <100000000>, <100000000>;
};
....
for your board dtsi.
I could not start the pcie-bus with the function Gen2.
Next, I needed to change the bus driver (pci-imx6.c), for fine tuning the bus clock frequency. I add MPLL frequency services functions (Thanks for Charle Powe i.MX6Q: Using an external reference for PCIe ):
...
static void imx_pcie_override_phy_mpll(struct pcie_port *pp, u32 mpll_multiplier, u32 ref_clkdiv2)
{
u32 ref_usb2_en;
u32 reg1;
pr_info("Overriding PCIe PHY MPLL config: multiplier = %d, clkdiv2 = %d\n",
mpll_multiplier, ref_clkdiv2);
// set MPLL to disabled
////pcie_phy_write(pp->dbi_base, PCIE_PHY_MPLL_OVRD_IN_LO, 0x0001);
// set MPLL multiplier
pcie_phy_write(pp->dbi_base, PCIE_PHY_MPLL_OVRD_IN_LO,
(0x0001<<9 | (mpll_multiplier<<2)) & 0x03fc);
/*
* set the ref_clkdiv2. when this override is enabled it
* overrides both ref_clkdiv2 and ref_usb2_en. make sure
* the overriden ref_usb2_en reflects the original value.
*/
pcie_phy_read(pp->dbi_base, PCIE_PHY_ATEOVRD, ®1);
ref_usb2_en = (reg1 >> 1) & 0x1;
/* set the current value of ref_usb2_en as the override */
/* set the ref_clkdiv2 override */
/* enable the ref_clkdiv2 override */
pcie_phy_write(pp->dbi_base, PCIE_PHY_ATEOVRD,
(ref_usb2_en << 1) | ref_clkdiv2 | (0x1 << 2));
/* enable MPLL */
///pcie_phy_write(pp->dbi_base, PCIE_PHY_MPLL_OVRD_IN_LO, 0x0003);
}
...
call this function in pcie_hos_init
...
static void imx6_pcie_host_init(struct pcie_port *pp)
{
imx6_pcie_assert_core_reset(pp);
imx6_pcie_init_phy(pp);
imx6_pcie_deassert_core_reset(pp);
imx_pcie_override_phy_mpll(pp, 50, 1); /* tune this */
dw_pcie_setup_rc(pp);
imx6_pcie_establish_link(pp);
if (IS_ENABLED(CONFIG_PCI_MSI))
dw_pcie_msi_init(pp);
}
...
See documentation for p.p. IMX6DLRM 50.5.1.2.
Tune <pci_hotplug_mem_size> global variable for optimal pci window sizes enumeration.
See for my imx6_add_pcie_port call.
If you use a FEC module, it will stop working. You must use an external clock as specified in the documentation (http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf ). Changes are shown in the attached dtsi file.
For clocks segment
...
rmii_clk: clock@0 {
compatible = "fixed-clock";
reg = <0>;
#clock-cells = <0>;
clock-frequency = <50000000>; /* 50MHz */
};
...
and for fec:
...
fec: ethernet@02188000 {
compatible = "fsl,imx6q-fec";
reg = <0x02188000 0x4000>;
interrupts-extended =
<&intc 0 118 IRQ_TYPE_LEVEL_HIGH>,
<&intc 0 119 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6QDL_CLK_ENET>,
<&clks IMX6QDL_CLK_ENET>,
<&rmii_clk>;
clock-names = "ipg", "ahb", "ptp";
status = "disabled";
};
...
If they are not required, disable this editing this file.
Thanks for all. Sorry for my bad English.
Alfred <[email protected]>
This document was generated from the following discussion: IMX6 PCI with external cloks