question about imx6 pcie's frequency/clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

question about imx6 pcie's frequency/clock

ソリューションへジャンプ
2,609件の閲覧回数
jiangyaqiang
Senior Contributor I

                                                                                 question about imx6 pcie's clock

      In the document of "reference manual", there are three source clocks for  phy_ref_output_clk, but how to select it ?

Refer as bellow:

pastedImage_1.png

linux version: 4.1.15

ラベル(5)
0 件の賞賛
返信
1 解決策
2,066件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jiang

by default 125MHz is used in imx6qdl.dtsi :

clks IMX6QDL_CLK_PCIE_REF_125M

linux-imx.git - i.MX Linux Kernel 

also other clocks may be selected as described on

IMX6 PCI with external clocks  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,067件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jiang

by default 125MHz is used in imx6qdl.dtsi :

clks IMX6QDL_CLK_PCIE_REF_125M

linux-imx.git - i.MX Linux Kernel 

also other clocks may be selected as described on

IMX6 PCI with external clocks  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信