MIPI DSI max display resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI DSI max display resolution

Jump to solution
4,438 Views
jotes
Contributor IV

What is the maximum display resolution for MIPI DSI?

Is it 1280x720 (as it is mentioned in IMX6DQRM Rev. 3, 07/2015) or is it 1024x768 (IMX6QLXRM Rev L3.0.35_4.1.0, 09/2013)?

We would like to connect the 1280x720 Super AMOLED display to our IMX6Q board, and we wonder if it has any chance to work correctly?

0 Kudos
Reply
1 Solution
3,306 Views
art
NXP Employee
NXP Employee

The maximum possible display resolution on the MIPI DSI interface of the i.MX6Dual/Quad processors is 1280x720 pixels, as specified in the Reference Manual document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,307 Views
art
NXP Employee
NXP Employee

The maximum possible display resolution on the MIPI DSI interface of the i.MX6Dual/Quad processors is 1280x720 pixels, as specified in the Reference Manual document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply